Command/Query
:DISPlay:TRACe{Tr}:Y:SCALe:PDIVision <numeric>
:DISPlay:TRACe{Tr}:Y:SCALe:PDIVision?
This command sets value of Y-axis scale per division.
|
Description |
Y-axis scale per division value. |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
20 |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":DISP:TRAC1:Y:SCAL:PDIV 20"
20 OUTPUT 717;":DISP:TRAC1:Y:SCAL:PDIV?"
30 ENTER 717;A
:DISPlay:TRACe{Tr}:X:SCALe:PDIVision
TDR/TDT > input box under the left knob (Under Vertical)